Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)

Smooth-running, lightweight ball bearings for guide rollers in labelling machines

Technical data

  • What was needed: Uninterrupted flow in the bottling process
  • Requirements: Smooth running of the ball bearings, no need for external lubricants, no maintenance
  • Material: xirodur® B180
  • Industry: Beverages sector
  • Success for the customer: Guide rollers from igus ensure a reliable service with excellent coefficients of wear and friction without interrupting the process.

Go to the labelling machine:With the Sleevematic labelling machine, labels are cut from the roll one at a time and then attached to the bottles. Once a roll of labels is depleted, it needs to be replaced by a new one without stopping the entire plant. Here the so-called "buffer conveyor" is used as a film storage, in which Krones employs xiros plastic ball bearings from igus.
Krones AG manufactures and distributes custom-made machinery, plants and systems for the food and beverages industry.


Problem

In the past, Krones AG relied on conventional metallic ball bearings, but these did not run smoothly enough and were too heavy. In addition, the rollers stopped sometimes and the label tape could not be attached correctly on the bottle. Downtimes increased, resulting in additional costs. The problem was in finding lightweight and maintenance-free ball bearing solutions that could ensure smooth running in the guide rollers.

Solution

Due to the decisive advantage of the smooth running, the xiros guide rollers from igus were approved. Depending on the size of the film storage device of the Sleevematic labelling machine, between 12 and 36 guide rollers are used. Two xiros fixed flange ball bearings are used per guide roller. Due to the low mass, the freedom from maintenance and the best coefficients of friction and wear of the plastic solution, the problems with metallic ball bearings have become a thing of the past. 



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH