Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)

Module Connect ensures fast maintenance in the packaging industry

Profile

  • What was needed: Fail-safe complete system for energy supply
  • Requirements: Small installation space, simple and fast maintenance, dependability
  • Products: readychain® harnessed energy chain, Module Connect
  • Fields of application: Mechanical engineering, packaging industry
  • Success for the customer: The customer received a complete system from igus that was ready to install and thoroughly tested, and was able to greatly reduce its maintenance times thanks to the Module Connect interface concept

About the automatic packaging machine GBK 440:GHD Hartmann offers machines for slicing, packaging, sealing and grouping as well as for the transport and handling of baked goods and foodstuffs. For a present day packaging machine for industrial bakery products, for example toasting bread, the appropriate power supply components had to be found. The automatic packaging machine GBK 440 offers the safe packaging and sealing of product bags in one operation. A wide variety of food formats can be packaged on the machine with short cycle times. The speed can be varied according to your requirements and application. The machine is designed for up to 80 cycles per minute.
Packaging machine GBK 440

The challenge

The machine operates at high stroke rates in a comparatively short installation space, which is why highly flexurally resistant cables were a must. In addition, a simple and time-saving solution had to be found for maintenance in order to reduce machine downtime. Moreover, the condition of the components needed to be recorded and maintenance and service operations needed to be made more predictable and efficient.

Solution

The limited installation space available for the energy chain required a very small bend radius of 63 mm maximum. For this reason, an E4.1L energy chain, which can absorb very high forces, is optimally suited for the application. In addition, highly flexible chainflex cables are used – the servo cable CF10.UL.05.04 with a minimum bend radius of 5xd, the control cable CF9.03.04.INI and the measuring system cable CF113.028.D. A 6-mm pneumatic hose and two other CF9 sensor cables complete the range, and the customer receives a ready-to-install and fully tested readychain system.


Maintenance was planned in advance with CF.Q. Sensors of various types record the status of the igus components and report this to the so-called icom module, which transfers the data to a cloud system. Thereby maintenance and service assignments become more predictable and therefore more efficient. The CF.Q module specifically monitors the cables used on the machine and informs the user at an early stage if a cable replacement is necessary.
Initial tests of the CF.Q System on the GBK 440 series machine indicate that the time interval until the next maintenance is expected to be significantly longer.
Module Connect interface concept in the packaging industry
In case of maintenance, igus has provided a plug-and-play system to enable quick maintenance. Previously, maintenance work took about four hours, which could often only be carried out by two employees. A replacement of the energy supply system now takes about 45 minutes with just one person using the new interface concept, the Module Connect from igus.
 
GHD Hartmann is one of the first customers to use the Module Connect connector. End customers of GHD Hartmann easily replace the energy supply with the plug-in connector from the modular system.
 
Find out more about Module Connect

motion - magazine for energy chain systems®

Improve the performance of your machine ... Cost down.

In this igus® magazine you will find numerous possibilities and application examples of how you can bring your tech up and/or cost down with ready-to-install energy chain systems.
Order your personal copy here


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH