Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)

The plastic energy chain guides 200kg/m cables on an offshore drilling vessel

A robust plastic e-chain ensures safe cable guidance for an offshore drill skid

This 3000HP modular offshore drilling rig has the world's largest plastic e-chain installed on a cantilever and the drill floor. Both energy chains were pre-assembled at our plant in Cologne so that they could be installed quickly on the drilling platform. Both travels (17.5m for the cantilever and 8m for the drill floor) bear an additional load of about 200kg/m.

Profile

  • What was needed: E4.1 series energy chains
  • Requirements: Given the 17.5m and 8m travel of cantilever and drilling floor skid, respectively, a safe cable guidance system for an additional load of 200kg/m was needed.
  • Industry: Oil and gas
  • Success for the customer: The plastic energy chains are designed to be strong and lightweight at the same time. This reduces the system's total weight. It is also particularly suitable for environmental conditions at sea (corrosion, wind, etc.)
Offshore energy chain Superlative energy chains: Despite high cable weights and enormous dimensions, the robust plastic energy chains safely move the drill floor skid and cantilever.

Problem

Modular drilling rigs are required for such situations as when drilling equipment needs to be added to fixed drilling platforms.
Mobile drilling vessels have all the necessary equipment for mooring at the drilling station and precisely placing the extended drill pipe. For this purpose, a huge cantilever moves over the drilling platform over which the drill pipe is finally to be set up and precisely positioned. Large cable guidance systems are required to ensure that the entire movable structure for setting up and placing the equipment can also move smoothly and without failing. In this application, the cantilever should be able to travel 17.5m, the mobile drilling floor 8m. The moving cables reach an additional load of 200kg/m, a major cable guidance challenge. The harsh conditions at sea meant that the solution needed to be particularly robust and durable, withstand corrosion, and have as little dead weight as possible.

Solution

Two of our E4.1 series plastic energy chains are used today to safely move the cantilever's cable load. Specifically, the E4.350 e-chain was chosen. It is the largest plastic energy chain installed on a cantilever and drilling floor.   It is not only strong, but also designed to use installation space optimally. This reduces weight and the drive energy required on the drilling rig. The heavy duty chains handle the heavy weight of the cantilever cables without any problem. Good preparation is also important for implementing such a project: Both energy chains were pre-assembled at our plant in Cologne so that they could be installed quickly on the drilling platform.
Offshore energy chain The chain could be installed quickly on the drilling vessel because the cable guidance system had been pre-assembled at our plant in Cologne.
Offshore energy chain The heavy cables on the drilling vessel required a particularly robust guidance system. This results in additional loads of about 200kg/m.

Here you can find the products used

E4.350 series

Inner height hi: 350mm
Inner widths Bi: 400-800mm
Bend radii R: 500-1000mm
Pitch: 470mm


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH