Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
My contact person
igus® Canada

180 Bass Pro Mills Drive

Concord

Ontario L4K 0G9

+1 (800) 965-2496
+1 905 760-8688
CA(FR)
Carousel washer
For freshly painted car parts
Order a free sample

Technical data:

  • What was needed: To automatically wash complex parts after painting in the automotive industry: this task is performed by the carousel washing system from the Polish manufacturer Noyen
  • Requirements: 100% lubrication-free and maintenance-free, withstands high humidity and high temperatures, lightweight, robust, accurate positioning, easy to retrofit
  • Products used: drylin® linear module SHT-20, with integrated dryspin® lead screw and lead screw nut
     
  • Success for the customer: An important design goal was to create the possibility of simple and ergonomic manual loading. The large number of references required not only suitable tools, but also actuator repositioning between references. This required a lockable, easy-to-operate, sliding mechanism. The solution had to be both lightweight, as it is built into a carousel, and robust. It was therefore decided to implement a new design with bearings.
Do you need more information? Contact us here
Rotating car wash brush system

Problem

NOYEN Expert C works in the final assembly line of parts that will be one of the most important components of the future vehicle. The washing process takes place after the parts are painted and before they are packed. Since most of the products manufactured in the factory have to pass through this production step, the machine had to meet the requirements for easy changeover and handling of all types of manufactured parts. Adapting the machine to handle dozens of different product references while maintaining the condition of easy changeover, as well as developing and implementing an innovative method for washing components for which cleanliness standards did not previously exist, were the major design challenges. Combined with the need to adjust the equipment to different references, special tools have been developed to allow the handling of any type of workpiece, its correct orientation during the washing process and a high repeatability of the pick-up and set-down positions required for automation processes. An important goal of the design was to create the possibility of easy and ergonomic manual loading. The large number of references required not only suitable tools, but also actuator repositioning between references. This required a lockable, easy-to-operate, sliding mechanism. The solution had to be both lightweight, as it is built into a carousel, which requires weight reduction, and also robust. It was therefore decided to implement a new design with bearings. Since the system is located inside the washing machine, the work of the components takes place at high temperatures and high humidity. In addition, the system is subject to impact loads from the robot or positioning inaccuracies of certain components of the complete workpiece, which can change their position under certain conditions. In addition, the system should be easy to change over and include position visualisation to reduce potential handling errors.

Solution

NOYEN Expert C series is a machine designed for industrial washing of parts. This solution was developed for the automotive manufacturer. It enables washing of the most complicated parts according to the highest cleanliness classes. The functionality of the plant was fully adapted to the customer's requirements. The number, type and duration of the processes were adjusted. The washing and drying processes were optimised by adapting the positioning of the washing and drying nozzles to the geometry of the workpiece and by separating the washing and rinsing chambers. The NOYEN Expert C washing machine guarantees high efficiency due to short cycle times of a few seconds and simultaneous execution of all sub-processes. The machine is characterised by its compact size, so it does not take up much space in the production hall. The machine is operated by a robot that makes it fully automatic. 

The igus products were used to adjust the height of the workpiece holders. They were placed directly on the carousel that transports the parts between processes within the machine. Two SHT tables were installed in each of the six sections. The variant used solved the problems associated with the complexity and costliness of the classic solution. At the same time, the new method is lighter and adapted to the more difficult conditions of an industrial washing plant. Benefits resulting from the implemented solution include:
  • The provision of the necessary regulatory parameters
  • Ergonomics
  • Significant reduction in manufacturing costs
  • Simplification of the construction
  • Weight reduction
  • Acceleration of the assembly of the entire device
  • Ensuring the repeatability of the components
  • Achieving a high level of freedom from defects
In addition, the system has been improved in terms of reliability. Furthermore, the system has gained in terms of visual appearance. It looks simple and solid. The finally applied solution has proved to be so good that it can be found operating in unchanged form in many machines, for example, in Mexico, China, Germany or in some equipment in Poland.

Further application pictures:

Rotating car wash brush system
3D
3D
3D
3D

Products used

drylin® SHT linear module

Lead Screw

dryspin® lead screw

Lead Screw

dryspin® lead screw nuts

Lead screw nut

dryspin® lead screw drives in vehicles

Five reasons why dryspin® technology is used in automobiles

With the dryspin lead screw technology, it is easy to design individual lead screw nuts and lead screws exactly according to the wishes of the customer. Our experts will be happy to help you choose the right lead screw drive and will ensure that deliver times are short. The wide choice of materials and complete absence of a need for lubrication or maintenance mean that the lead screw drives can be used in almost any area of the automotive industry. They are ideal for small installation spaces and operate almost silently even when the drive torque is low. Uncomplicated integration into your vehicle or assembly is also an aspect that speaks in favour of the cost-effective alternative to conventional lead screw drives made of metal. 
Automotive

Do you have questions about drylin® lead screw technology?

Our expert, Thorben Hendricks, will answer all your questions about dryspin lead screw technology. Just fill out the contact form, and we will address your concerns. We are looking forward to your message!
► Request contact online
► Make an appointment
► Expert support upon request by phone or with the video chat function
► Order a free sample
 
Request expert support here

Configure lead screw drive:

Filling system

Improve technology ... reduce costs:

Tech up, Cost down



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH