180 Bass Pro Mills Drive
Concord
Ontario L4K 0G9
Watch the video to find out how we are already actively making a difference.
Our customer BSH Hausgeräte was looking for a solution that would enable them to efficiently unwind cables, avoid waste during maintenance, and save packaging material.
The solution was the chainflex CASE! Thanks to this solution, our customer could simply unwind the cables directly from the case in the warehouse, avoid unnecessary waste and was able to save 84% in shipping costs due to using a local courrier.
What is good for our customers is also good for the environment.
The customer was satisfied with this solution and we, in turn, were proud to have also protected the environment. Packaging materials were saved in the long term and no waste was produced due to offcuts. They also had and have the possibility of using the refill option and could save yet another 2.6kg of packaging waste.
This test case was an absolute win-win for igus and the customer.
Energy supply can be a challenge, especially on long travels.
Customers do not want to spend a lot of money unnecessarily, especially on cable replacement. Further disadvantages on short use cables is the growth of waste from old cables and the high energy consumption for producing new ones, in addition to the journey from production to use.
One of our customers faced these problems in an application with an indoor crane in a cement plant with a 32m crane runway.
Save money and protect the environment.
The solution included an energy chain filled with various chainflex cables. The guaranteed durability ensured functionality, which saved customers time and money while conserving valuable environmental resources.
At the heart of our sustainability efforts lies our commitment to producing high-quality, durable products. Our rigorous testing and continuous quality checks ensure that our cables stand the test of time. We proudly offer cables with a guarantee of up to four years, significantly reducing the need for frequent replacements.
Our 4-year guarantee is not merely a marketing claim. It is UL-verified, underscoring our dedication to providing reliable and trustworthy products.