drylin® T Automatic: Adjusting the clearance

With drylin® T Automatic, the bearing clearance is automatically adjusted. A re-adjustment can take place automatically in steps of 0.004” (0.1 mm). Springs tighten the regulating wedge immediately as soon as the clearance is bigger than 0.1 mm and the system is unloaded.
Locked
Unlocked

The system will be delivered with three red keys which are already fitted in the carriage. These are necessary for mounting the carriage onto the rail. In case these keys are removed, they need to be re-plugged into the openings and turned 90° clockwise.
When the carriage is on the rail, remove the keys by turning them 90° anticlockwise and pulling them out. The clearance will then be adjusted automatically.
Check the clearance of the carriage. Fine adjusting can be done at this point.
You can remove the carriage at any time. In order to do so, simply plug the keys back into the cariage (see first step).


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH