/wpck/10887/sample_dry_tech

Request an igus® dry-tech® box... It's FREE!


igus® iglide® bearings

Discover igus® dry-tech® solutions

Worldwide, more than 50% of lubricants are discharged into the environment.
(State of Baden-Württemberg Environmental Protection Agency)
 

At a world-wide lubricant consumption of 37.3 million tons annually, this results in more than 18 million tons of uncontrolled discharge into the environment
RWTH Aachen)
 

Malfunctions due to deficient lubrication cause $240 billion in damage in the US alone
(MIT), Massachusetts Institute of Technology
igus® metal vs. plastic bearing
The right plain bearing...
... for every application
 
... made of plastics
 
... lubrication-free
 
... tested and predictable
 
... dirt-resistant and corrosion-free
 
... lightweight and quiet
 
... Reduce costs and increase service life
 
... extensive standard product range and individual design
 
... delivered from stock in 24 hours
 

How does it work?

The base polymer is crucial for wear resistance.
Fibers and filling materials reinforce the bearing to take high forces or edge loads.
Finally the solid lubricants self-lubricate the bearings and prevent friction in the system.

Their product advantages are their technical properties

How it works

Lubrication-free and hygienic

Self-Lubricating and Maintenance-Free

Cost saving offered through elimination of maintenance work

Avoidance of lubricants

No central lubrication system required

No downtime

igus® tested

igus® iglide® test lab

igus® operates the largest laboratory of its industry with over 200 test stands for varied types of application and loading scenarios.

Application examples

Industrial variety

The iglide® plain bearing application spectrum ranges from applications in packaging and medical technology, which avoid lubricants for hygiene reasons, to highly contaminated applications, ex. in agricultural engineering.

How it works

High wear resistance

igus® develops special plastics - triboplastics - that are optimized for various applications with respect to wear and as a result the service life.

igus® tested

High variety testing

Testing on various shafts determines the materials with the longest service life for any application - whether rotating, pivoting, linear, fast or slow, high or low loads, dry or submerged.

Application example

Bottling carousel
in continuous operation

"Bearing materials marked by special properties such as low coefficients of friction in dry operation, chemical resistance and low humidity absorption in equal measure are best suited for the application in high-tech beverage bottling plants. ”
 
Bernfried Götz, KHS AG, Monzingen

How it works

Resistant against dirt and dust

Resistant against dirt and dust

iglide® plain bearings are very robust in contaminated environments, primarily because lubricants are avoided. - Dirt particles do not adhere to a lubricant coating on the shaft or the bearing location. - Dirt can even be partially embedded. In place of a soft and thin gliding surface that can easily be damaged by abrasive particles, there is a homogeneous material structure across the entire wall thickness.

igus® tested

Good for the shaft

1. Wear rate [µm/km]
2. iglide® Q
3. iglide® G300
4. iglide® Z
5. Brass with initial lubrication
6. Rolled metal with gliding layer
 
A host of tests in the igus® tribo lab show what has been confirmed in field through use in industries such as agricultural engineering, wood processing, construction machinery, etc.: iglide® plastic plain bearings are rugged and have a long service life even under the most adverse conditions, while also protecting the shaft.

Application example

Hay spreader

The external demands on custom bearings developed by igus® when used on the job during Summer are extremely high. "These primarily involve radial forces", explains the design engineering manager at FELLA-Werke GmbH, Grad. Eng. (FH) Bernhard Kohl. In order to protect plain bearings against damage from these crash events, they must be impact-resistant and very robust. “ Then there is dust and dirt plus finally high pressure washing. “Rough conditions and long service lives with possible corrosion on the steel parts place very high demands on the plastic bearings,” says Bernhard Kohl.

How it works

Lubrication-free and hygienic

Lubrication-free and hygienic

The dry-running properties of iglide® plain bearings are not only advantageous in contaminated environments. The absence of lubrication is also an important criterion in applications with elevated requirements for hygiene and purity.

igus® tested

iglide® standard tests

All standard tests at the igus® tribo lab are conducted without lubricants. Only special customer-specific tests are conducted with contact to media - incl. lubricants when appropriate. This approach allows us to optimize our materials for dry running conditions, and we therefore know in detail what service life can be expected.

Application example

Secure under high forces

Bearings L280 and iglide® Q are seated in all bearing points of the artificial knee joint. The bearings require no maintenance, operate without clearance and exhibit only minimal wear. Moreover, they should run free of noise, dampen impacts and have a good price/performance ratio.

How it works

Corrosion and media resistant

Corrosion and media resistant

All iglide® plastic plain bearings are by their nature corrosion-free. There are also special purpose materials, which can be used in caustic solutions, acids, cleaning agents, etc., and, due to their media resistance, can be used even under the most adverse conditions. - The product range also has special purpose materials for permanent use in submerged conditions.

igus® tested

Submerged testing

Submerged testing in the igus® tribolab has resulted in iglide® materials that play to their strengths primarily in these specialized applications. - In this case, the medium is not necessarily always water; other liquid media are also used.

Application example

Use in corrosive environments

The enormous increase in service life of the roller chain is due to its special joint structure. A high-performance polymer bearing from igus® was integrated in a stainless steel carrier bushing, "which significantly enhanced the tribology of the chain joint." According to the customer's statement, "the plastic plain bearings raise the bar with extremely high wear resistance, a low friction value, high compressive strength, and chemical resistance." “

How it works

Light

Light

Weight reduction plays an important role in a host of applications, which plastic bearings are ideally equipped to address. - This could involve the need to attain an increase in energy efficiency, or to increase cycle rates and speeds.

igus® tested

Weighing in

Due to their low material density, plastic plain bearings have significant advantages compared to metallic alternatives with respect to the topic of weight reduction.

Application example

Aircraft interior industry

For instance, weight reduction plays a predominant role in aviation. In this case, the use of plastic plain bearings in the seat kinematics, luggage panels, food trays and other applications in the cabin area is helping to achieve significant weight reductions.

How it works

Quiet

Quiet operation is primarily of significance where people are directly affected. Comfort and well-being are materially impacted by background noise.

igus® tested

All ears

The igus® tribo lab is all ears when it comes to the topic of noise profile. After all, what use is an unlubricated plain bearings with a long service life when it screeches and grinds?

Application example

No noise

"A gliding body was required to fulfill the following functions: It should glide on drawn aluminum profile (column), the material must be abrasion resistant, the gliding movement should be free of noise, the gliding body cannot leave behind traces and it should possess a ten-year service life. After several rejected solution proposals, only the material from igus® remains. It began functioning at first go, and five years have passed since. ”
Hanna Tielebier, Carl Zeiss AG, Jena

The right iglide® material

igus® test lab
iglide® product finder
Expansive wear data from more than 15,000 tests each year under various conditions help to identify the ideal material for any application.
Determine your ideal bearing material - on your own, or with our assistance. Using the iglide® product finder and the iglide® service life calculator.

Order from stock

All-rounder

Long service life

High temperatures

High media resistance

Food contact

Special applications

More plain bearing designs

Want to learn more? Receive a free dry-tech® bearings box!



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH