180 Bass Pro Mills Drive
Concord
Ontario L4K 0G9
iglide® plastic bushing materials consist of base plastics, fibers and filling materials, and solid lubricants. These components are not applied in layers, but homogeneously compounded.
The advantage of this construction becomes clear if you consider the following:
1. The coefficient of friction, determined by the surface of the plastic bushing, should be as low as possible
2. The surface must not be pushed aside by forces acting on the plastic bushing
3. The plastic bushing should be particularly resistant to wear forces acting on its surface.
There is no universal material available that can fulfill all these tasks equally well.
In the initial phase, the shaft and the iglide® plastic bushing become mated to one another. During this period, the surfaces of both partners are fitted to each other. The specific load of the system lowers as the contact surfaces of the shaft and plastic bushing expand during start-up. Simultaneously, the wear rate lowers and approaches a linear curve. In this phase, the coefficients of friction continue to change, until finally assuming a value that is - for the most part - constant.