Chain, cable, plug: Ready-to-install energy supply in SAMAG machine tool

SAMAG saves 2/3 assembly time thanks to readychain® Premium


A large machining volume, up to 40m/min machining speed and 5m/s² acceleration. Available as a 3-, 4- or 5-axis version, the long-bed machine tool of the SFZ series from SAMAG is designed for high stiffness, stability and performance. The same requirements also applied to the e-chain®. Thanks to readychain® energy supply, which was fully equipped with assembled cables including plug connections, the customer saves 2/3 of the assembly time and considerable costs.
 

Profile

  • Industry: Machine Tools
  • Requirements: High reliability and robustness of chips and cooling lubricants as well as high machine performance. Small installation space. Fast and cost-effective installation of the entire system.
  • What was used:
    e-chain® E4Q as ready-made readychain® (readychain Premium)
  • Result: After precise design of the energy supply for SAMAG by our project team, the customer was able to save 2/3 of his usual assembly time.
Learn more about machine tools
Werkzeugmaschine von SAMAG

Problem

The SAMAG SFZ series is a completely newly developed long-bed machine tool in travel column design. The Y and Z axes have a travel of 1,000 mm. And the X travel can be selected in four steps from 2,500 mm to 7,500 mm. Particular attention was paid to high rigidity and stability as well as high performance, which achieves a large machining volume. The machining takes place at up to 40m/min and an acceleration of 5m/s²- For this reason, a cable routing should also be found for all three linearly moving axes, which can insist on a broad portfolio of requirements. In the environmental conditions of a typical industrial production, which is characterized by chips and cooling lubricants, a long service life and reliability of the energy supply should be guaranteed. Maintenance intervals are to be extended and planning security is to be increased. Since space in machine tools is always tight, the cable routing also had to be compactly designed. Most recently, solutions were sought that ensure fast assembly and thus low organizational costs.

Solution

SAMAG found what it was looking for in our E4Q.82 series e-chains as a pre-assembled readychain energy chain system. Thanks to the cable routing of the readychain Premium version, which is already fully equipped with cables and plugs, the assembly time on the machine could be reduced by approx. 2/3. At the beginning of the project, SAMAG provided us with all the necessary parameters, such as the required cables and hoses, their assembly, the length of the travel distances or the space available. As a result, the machine specialist was able to save not only an increased expenditure of time but also a greater organizational effort. After close planning by our project team together with the contact persons of Samag Machine Tool GmbH, the first and second prototypes were installed at the customer's site together with the assembly management, optimizations were developed and implemented promptly.
Learn more about readychain® Pre-Assembled Cable Carriers
Werkzeugmaschine von SAMAG
readychain rack premium Energiekette


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH