Assembly instructions triflex® RSP

Mounting with adapter plate

The triflex® RSP system requires a mounting adapter for most robot models. triflex® RSP systems can be mounted to some Kuka robots with an adapter.
RSP assembly Click to enlarge

Mount Adapter plate

Assemble adapter plate (1) onto axis 3 of the robot
rsp_02 Click to enlarge

Mount the triflex® RSP system

Assemble the igus® RSP system directly onto a) the adapter plate (1) or b) directly onto your robot if an adapter plate is not needed.
rsp Click to enlarge

Mount the "tennis racket"

Mount the "tennis racket" (2) on axis 6 of the robot and then the adjustable triflex® R mounting bracket to the shaft (3)
Note: Mounting bracket will be delivered as a complete assembled set.

Adjust length

rsp_04 Click to enlarge

Install triflex® R E-Chain®

Fit your triflex® R E-Chain® into the  RSP system 
rsp_05 Click to enlarge

Adjust the length

Adjust the length of triflex® R chain and attach it to the fixed point of the RSP system and at the moving end at axis 6.
rsp_06 Click to enlarge

Align

Note: for triflex® TRE only. Please install lock clips at all fixed bracket locations

Pressure compensation

rsp_07 Click to enlarge

Adjust tennis racket

The tennis racket and axis 6 bracket can be adjusted in several angles to suit the robot motion.
rsp_08 Click to enlarge

Connect the pressure equalizing unit

Connect the supplied 1m hose (red) to the RSP unit. The other line is your air supply (green) and is attached to your compressed air system.
rsp_09 Click to enlarge

Adjust air pressure

Adjust air pressure using pressure reducing valve. The correct pressure is between 2 (29 PSI) and 4 bar (87 PSI).
rsp_10 Click to enlarge

Optimal setting

For the most accurate pressure setting fill the triflex® R with cables and hoses and run the robot in a vertical position with axis 6 downwards.

Increase the air pressure until the wheel returns to the home position (F).

Take note of the pressure required to return the wheel to the home position. This setting is the maximum force required and should not be increased.

triflex® RS troubleshooting guide

ProblemSolution
RSP System does not have enough tension to retract the dresspack
  • The air pressure is too low. Remove the air from the system and repeat step 8, 9 & 10 from the install manual
RSP System has too much tension and the triflex® R is breaking
  • The air pressure is too high. Remove the air from the system and repeat step 8, 9 & 10 from the install manual

Discuss your project with a triflex® R expert

We can assist you with a turnkey, fully assembled solutions or answer any questions you may have with a custom project. 

David Sandiland
Robotics Sales Manager - North America
(705) 313-2574
Contact an igus® expert now

Overview of Assembly Instructions for igus® e-chains®



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH