Where to Use Cost-effective Continuous-flex Cables
You may have heard us say it before, but helpful tips are always worth repeating: it is important to use cables specifically designed for continuous flexing in demanding, high-cycle applications.

However, not every application is as demanding as the next. In these instances where a low- to medium-duty continuous-flex cable can be used, there are some attractive cost-effective options.
Cost-effective Continuous-flex Cables 1.1: In certain low- to medium-duty applications, cost-effective continuous-flex cables can be used.

Applications

First, let’s review some specific applications that could benefit from cost-effective continuous-flex cables. Of course, every application has its own set of unique parameters, but generally a less expensive continuous-flex cable can be used in the following areas:

  1. Machine tools Certain types of machine tools, such as water jet and laser cutters, move at slower speeds which subject cables to a lower duty cycle. Also, the configuration of the cable carrier is sometimes short enough where the top section does not need support. Therefore, as long as the cable has an adequate bend radius, an industrial, higher-cost continuous-flex cable is not needed. Instead, a medium-duty continuous-flex cable that is able to withstand light abrasion and exposure to oils is ideal.

  2. Packaging and handling systems Depending on the industry, some packaging and handling machines are required to run at reduced speeds. Similar to a machine tool application, a cost-effective continuous-flex cable that is able to withstand light abrasion and occasional exposure to oils is ideal.

  3. Small gantry cranes Typically gantry cranes are used to lift and transport smaller items around a working area in a factory or machine shop. Where a larger bridge or overhead cranes may require industrial, higher-cost continuous-flex cables, gantry cranes can often use a cost-effective continuous-flex cable because of their shorter length of travel and slower operational speeds.

  4. Car washes An automatic car wash does not put undue stress on cables, as they handle only light to medium loads. While the cables still need to be rated for continuous flexing, a less expensive continuous-flex cable that is suitable for outdoor use in a range of temperatures can be used.

Cost-effective Continuous-flex Cables

Now that we have discussed potential applications for cost-effective continuous-flex cables, let’s review the features and benefits of the cables themselves. Below are some examples of cost-effective continuous-flex cables for medium-duty applications offered by igus®. Based on pricing and performance features, these cables would be considered “economy”, while the higher priced, more robust cables also offered by igus® would be considered “standard” or “premium”. For an overview of igus®' entire line of chainflex® cables, visit our website.

Servo Cables

Chainflex® CF210 continuous-flex cables

  • Ideal for medium loads and unsupported travel lengths
  • PVC jacket
  • Recommended for indoor applications, but can be used outdoors in temperatures above 41 degrees Fahrenheit
  • Withstands light exposure to oils
  • Bend radius: 10 times the outer cable diameter
  • Applications: wood / stone processing, packaging and handling, adjustment equipment
Chainflex CF210 Servo Cables

Chainflex® CF270 continuous-flex cables

  • Ideal for medium loads and unsupported travel lengths
  • PUR jacket
  • Recommended for indoor and outdoor applications without direct sunlight
  • Oil and coolant resistant
  • Flame retardant
  • For temperatures from -40 degrees Fahrenheit to +176 degrees Fahrenheit
  • Bend radius: 7.5 times the outer cable diameter
  • Applications: machine tools, quick handling, clean room
Chainflex® CF270 Servo Cable

Measuring Cables

Chainflex® CF113 continuous-flex cables

  • Ideal for high loads and unsupported / gliding travel lengths up to 1,312 feet
  • PUR jacket
  • For indoor and outdoor applications (UV resistant)
  • Oil and coolant resistant
  • Flame retardant
  • For temperatures from -40 degrees Fahrenheit to +176 degrees Fahrenheit
  • Bend radius: 7.5 times the outer cable diameter
  • Applications: machine tools, quick handling, clean room, cranes, car washes
Chainflex CF113 Measuring Cable

Chainflex® CF211 continuous-flex cables

  • Ideal for medium loads and unsupported travel lengths
  • PVC jacket
  • Recommended for indoor applications, but can be used outdoors in temperatures above 41 degrees Fahrenheit
  • Oil resistant
  • Flame retardant
  • Bend radius: 7.5 times the outer cable diameter (CF211standard version)
  • Applications: storage and retrieval units, packaging machines, indoor / gantry cranes
Chainflex CF211 Measuring Cable

Useful Links and Tools



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH