Flexible 3D energy chains as cable routing to riveting robots for aircraft construction


In aircraft construction, the e-chains carry a high cable weight during fast robot movements.

LOXIN 2002 succeeded in automating riveting. The multi-axis robots are located to the left and right of the jacked-up fuselage in production at a large aircraft manufacturer. The robots are mounted on platforms that can be moved to a height of several meters via linear units. Once at the right height, the robot moves to the operating point with millimeter precision over six axes. He drills a hole in the metal, mills a sink for the rivet head, sucks off the dust, applies sealant and places the rivet.

Profile

  • What was needed: 3D energy chain system triflex R with retraction system triflex RSE, twisterchain
  • Requirements: Reduce the number and weight of cables, avoid downtime and cable breaks
  • Industry: Aerospace, aircraft construction
  • Success for the customer: Thanks to triflex 3D cable guides, the robots achieve better mobility, which saves assembly time.

Problem

LOXIN, a member of the ARITEX Group, was looking for a suitable solution for the energy supply system for the multi-axis robots. The problem, however, was to find a line solution that was reliable, resilient and trustworthy at the same time. This was aggravated by a high number and the resulting high weight of the cables to be routed. The tools on the end effector of the robots are connected to numerous energy, pneumatic and data cables. These cables must be able to perfectly follow the dislocations of the arm, even at high speed. LOXIN used conventional corrugated pipes in the past, but these did not turn out to be a solution. Due to the rapid wear due to friction, they are broken in many places, which would have led to the entire replacement of the pipe including line dismantling during operation. The result: several days of machine downtime.
triflex® R Robot Dress Packs

Solution

LOXIN chose our triflex range. The hose-like protective cages made of wear-resistant plastic follow even the most extreme 3D movements of industrial robots. The cables are protected against mechanical stress caused by tensile load, twisting and expansion. With the triflex RSE retraction system, the energy chains move close to the arm and thus do not hit the aircraft. If the robot arm returns to its original position after movement, the mechanical system retracts the chain. The robot arm is guaranteed full freedom of movement without parts of the chain rubbing against each other or forming loops. Should a chain link reach the end of its service life, quick and easy replacement is possible. With the twisterchain, another energy chain system from us is used on the robot arm. It protects cables from the foot of the robot arm to the first axis, moving in a guide trough. When the robot arm rotates, the chain folds so that the upper run of the chain rests on the lower trot. In this way, a circular movement of up to 540° is realized at speeds of up to 1 m/s. The twisterchain is extremely wear-resistant and the proven service life is over one million cycles.

Nietroboter
twisterchain Nietroboter

Discuss your project with a triflex® expert

We can assist you with a turnkey, fully assembled solutions or answer any questions you may have with a custom project. 

David Sandiland
Robotics Sales Manager - North America
(705) 313-2574 
Contact an igus® expert now


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH