The Proof is in the Plastic
I’m sure you’ve heard the saying, “The proof is in the pudding.” But when it comes to self-lubricating plastic bearings, the proof is definitely in the plastic.
Over the past few decades, there has been a notable shift from recirculating ball bearings and PTFE-lined aluminum shells to high-performance plastic liners. This transition can be attributed to a number of factors, but two of the most important are material composition and the unique geometry of the replaceable liner.
Exposed plastic liner on a DryLin linear bearing 1.1: drylin® liners do not require any lubrication, which virtually eliminates maintenance.

Material Composition

During bearing operation, a wet lubricant is typically applied to reduce friction and minimize wear. However, igus®’ plastics inherently contain solid lubricant as particles released in small amounts during movement. As a result, all igus® bearings do not require any external lubrication, which virtually eliminates maintenance and lowers costs.
DryLin R high-performance plastic liner
drylin® R liners Material: iglide® J
Color: yellow
Suitable shafting materials: case-hardened steel, stainless steel, soft stainless steel, and anodized aluminum shafting

DryLin W high-performance plastic liner
drylin® W liners Material: iglide® J200
Color: dark grey
Suitable shafting materials: anodized aluminum shafting
DryLin T500 high-performance plastic liner
drylin® T500 liners Material: iglide® T500 (for high-temperature applications up to 482° F)
Color: dark grey
Suitable shafting materials: chrome-plated and hardened stainless shafts

Geometry

Aside from their material composition, the geometry of the plastic liners also makes them unique. The liner may look deceptively simple, but in fact, it is not.
The part has a lengthwise slit which enables easy installation into a housing bore without any tools; this is also known as “slip-fit”. Unlike press-fit bearings, a slip-fit bearing has raised ridges on the OD of the liner that create a mechanical stop in the housing. This eliminates the risk of the liner shifting due to temperature changes or extreme axial loading. There is also a large pin on the OD of the liner that secures it radially to keep it from rotating.
Geometry of DryLin plastic liners
DryLin® liners in harsh environment 1.2 drylin® liners have grooves that act like dirt channels so dirt and debris can easily pass through.
In addition, because of the slip-fit design, igus® is able to offer additional options. One example is the TJUI adapter, which makes bearing replacement possible without disassembling the shafts. Quick, easy liner replacement isn’t an option with a PTFE-lined bearing or ball bearing and is especially helpful in extremely harsh environments.

Lastly, the liner’s patented grooves serve two important purposes. First, if thermal expansion occurs, the grooves swell away from the shaft, which prevents the bearing from seizing. Second, in especially aggressive environments, the grooves act as dirt channels so dirt and debris can easily pass through the bearing system.

Are you currently working on an application where DryLin linear bearings or guides could replace PTFE-lined bearings or ball bearings? If so, I would love to help so e-mail me at mmowry@igus.com.

Useful Links and Tools



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH